Part Number: THVD1500
Other Parts Discussed in Thread: THVD1419, SN65HVD3082E
HI Sir
Could you help to share the Competitor table between AZRS3082.RDG,SH65HVD3082EDR,THVD1500DR
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1500
Other Parts Discussed in Thread: THVD1419, SN65HVD3082E
HI Sir
Could you help to share the Competitor table between AZRS3082.RDG,SH65HVD3082EDR,THVD1500DR
thanks
Hi,
THVD1419 might be a better match for AZRS3082, since both have surge protection feature. Here is the comparison among all 4 devices.
| Device | SN65HVD3082E | THVD1500 | ARZS3082 | THVD1419 | |
| Duplex | Half | Half | Half | Half | |
| Number of TX | 1 | 1 | 1 | 1 | |
| Number of RX | 1 | 1 | 1 | 1 | |
| Supply voltage(s) (Nom) (V) | 5 | 5 | 5 | 3.3, 5 |
|
| Signaling rate (Max) (Mbps) | 0.2 | 0.5 | 0.115 | 0.25 | |
| Fault protection | Feature - Extended Fault protection | NO | NO | NO | NO |
| Fault protection (V) | -9 to 14 | -18 to 18 | -13 to 13 | -15 to 15 | |
| Integrated IEC ESD protection | Feature - Integrated IEC ESD protection | NO | YES | YES | YES |
| IEC 61000-4-2 Contact Discharge (+/- kV) | Need external circuit | 8 | 30 | 8 | |
| IEC61000-4-2 Air-gap Discharge (+/- kV) | Need external circuit | 10 | 30 | 30 | |
| Integrated IEC EFT (Noise Immunity) | Feature - Integrated IEC EFT (Noise Immunity) | NO | YES | YES | YES |
| IEC61000-4-4 EFT (+/- kV) | Need external circuit | 2 | 4 | 4 | |
| Integrated IEC Surge Protection | Feature - Integrated Surge protection | NO | NO | YES | YES |
| IEC61000-4-5 Surge (+/- kV) | Need external circuit | Need external circuit | 1.26 | 2.5 | |
| Extended Common Mode | Feature - Extended common mode | NO | NO | NO | YES |
| Common mode range (V) | -7 to 12 | -7 to 12 | -7 to 12 | -12 to 12 | |
| Number of nodes | 256 | 256 | 256 | 256 | |
| HBM ESD (kV) | 15 | 16 | 15 | 16 | |
| ICC (Max) (mA) | 0.9 | 0.66 | 0.6 | 3 | |
| Temperature Range (°C) | -40 to 85 | -40 to 125 | -40 to 85 | -40 to 125 | |
Regards,
Hao