This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC811R-Q1: What is the delay between SFD symbol on the line and the assertion of the GPIO pins for IEEE 1588 indication pulse

Part Number: DP83TC811R-Q1
The DP83TC811R supports outputting a signal corresponding to rx/tx SFD on the GPIO signal: the datasheet refers to this as an "IEEE 1588 indication pulse".
It is assumed that a fixed delay between the actual SFD symbol on the line and the assertion of the GPIO pins exists (based on a similar feature on the DP93640 PHY).
Are these fixed delays specified anywhere for the transmit and receive GPIO indications?