This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH949-Q1: Questions regarding HDCP authentication

Part Number: DS90UH949-Q1

Hi 

in our system we are using DS90UH949 + DS90UH940. Our setup are HDMI input --> DS90UH949 --> DS90UH940 --> graphic processor 

Some quick question would like to clarify as below: 

1. after power on we had already done the procedure for DS90UH949 --> DS90UH940 HDCP authentication, and the status now are  DS90UH949 --> DS90UH940 HDCP authenticated. if the HDMI input is removed and plug in again does  DS90UH949 --> DS90UH940 need to re-do the HDCP authentication procedure (Enable HDCP -> Check for KSV Ready -> Check KSV., ...)

2. We saw that If DS90UH949 --> DS90UH940 HDCP is at authenticated status, if at this time we set DS90UH949  HDCP_CTL register HDCP_EN bit 0xC3[0] = 1 try to restart the authentication, the KSV Ready bit 0xC4[1] will not go high. Looks like it does not re-start the authentication.

         Why KSV ready will not goes high ?       

May I know what is the correct way to restart the authentication in this case ?