Part Number: TCAN4550
Hi Expert,
Customer is currently using Linux 2.6. They made some change based on the linux 5.8 related driver code in the processor. During the debug process, it can receive the data successfully when setting TCAN4550 in loopback mode. While when setting it to normal mode, the received results are all 0. I see there is another post on E2E that said the driver was introduced in Kernel version 5.4 and backporting to earlier versions would need to be done manually. Could you tell what steps the customer should do to make it work on Linux 2.6? The customer's code is as the attachment. Could you help check what may cause the issue?