Part Number: DS110DF410EVM
Other Parts Discussed in Thread: DS110DF410
Hi all,
For my setup at the moment I have a 644.53125MHz input into the DS110DF410EVM PRBS on one channel through SMA and output as 10.3125MHz. This channel is setup as below.
I use this setup with the register set below to program the card.
When I have address 0x18 set for divide by 8 or 16 the CDR can lock and I see PRBS data out from the device at the lower datarates.
However when I set 0x18 to divide by 1 and use 0x09 set of DIV_SEL to make this change I see PRBS data out but the CDR lock is lost.
Do you understand why this may be happening? Please find the channel register set below.
{0x00, 0x00, 0xFF},
{0x01, 0x00, 0xFF},
{0x02, 0xDC, 0xFF},
{0x03, 0xA5, 0xFF},
{0x04, 0x00, 0xFF},
{0x05, 0x00, 0xFF},
{0x06, 0x00, 0xFF},
{0x07, 0x00, 0xFF},
{0x08, 0x00, 0xFF},
{0x09, 0x20, 0xFF},
{0x0A, 0x10, 0xFF},
{0x0B, 0x0F, 0xFF},
{0x0C, 0x08, 0xFF},
{0x0D, 0x20, 0xFF},
{0x0E, 0x93, 0xFF},
{0x0F, 0x69, 0xFF},
{0x10, 0x3A, 0xFF},
{0x11, 0x20, 0xFF},
{0x12, 0xA0, 0xFF},
{0x13, 0x30, 0xFF},
{0x14, 0x00, 0xFF},
{0x15, 0x10, 0xFF},
{0x16, 0x7A, 0xFF},
{0x17, 0x36, 0xFF},
{0x18, 0x40, 0xFF},
{0x19, 0x23, 0xFF},
{0x1A, 0x00, 0xFF},
{0x1B, 0x03, 0xFF},
{0x1C, 0x24, 0xFF},
{0x1D, 0x00, 0xFF},
{0x1E, 0x99, 0xFF},
{0x1F, 0x55, 0xFF},
{0x20, 0x00, 0xFF},
{0x21, 0x00, 0xFF},
{0x22, 0x00, 0xFF},
{0x23, 0x40, 0xFF},
{0x24, 0x00, 0xFF},
{0x25, 0x00, 0xFF},
{0x26, 0x00, 0xFF},
{0x27, 0x3E, 0xFF},
{0x28, 0x9C, 0xFF},
{0x29, 0x40, 0xFF},
{0x2A, 0x30, 0xFF},
{0x2B, 0x00, 0xFF},
{0x2C, 0x72, 0xFF},
{0x2D, 0x80, 0xFF},
{0x2E, 0x00, 0xFF},
{0x2F, 0x06, 0xFF},
{0x30, 0x0A, 0xFF},
{0x31, 0x20, 0xFF},
{0x32, 0x11, 0xFF},
{0x33, 0x88, 0xFF},
{0x34, 0xBF, 0xFF},
{0x35, 0x1F, 0xFF},
{0x36, 0x31, 0xFF},
{0x37, 0x00, 0xFF},
{0x38, 0x00, 0xFF},
{0x39, 0x00, 0xFF},
{0x3A, 0xA5, 0xFF},
{0x3B, 0x00, 0xFF},
{0x3C, 0x00, 0xFF},
{0x3D, 0x00, 0xFF},
{0x3E, 0x80, 0xFF},
{0x3F, 0x00, 0xFF},
{0x40, 0x00, 0xFF},
{0x41, 0x01, 0xFF},
{0x42, 0x04, 0xFF},
{0x43, 0x10, 0xFF},
{0x44, 0x40, 0xFF},
{0x45, 0x08, 0xFF},
{0x46, 0x02, 0xFF},
{0x47, 0x80, 0xFF},
{0x48, 0x03, 0xFF},
{0x49, 0x0C, 0xFF},
{0x4A, 0x30, 0xFF},
{0x4B, 0x41, 0xFF},
{0x4C, 0x50, 0xFF},
{0x4D, 0xC0, 0xFF},
{0x4E, 0x60, 0xFF},
{0x4F, 0x90, 0xFF},
{0x50, 0x88, 0xFF},
{0x51, 0x82, 0xFF},
{0x52, 0xA0, 0xFF},
{0x53, 0x46, 0xFF},
{0x54, 0x52, 0xFF},
{0x55, 0x8C, 0xFF},
{0x56, 0xB0, 0xFF},
{0x57, 0xC8, 0xFF},
{0x58, 0x57, 0xFF},
{0x59, 0x5D, 0xFF},
{0x5A, 0x69, 0xFF},
{0x5B, 0x75, 0xFF},
{0x5C, 0xD5, 0xFF},
{0x5D, 0x99, 0xFF},
{0x5E, 0x96, 0xFF},
{0x5F, 0xA5, 0xFF},
{0x60, 0x90, 0xFF},
{0x61, 0xB3, 0xFF},
{0x62, 0x90, 0xFF},
{0x63, 0xB3, 0xFF},
{0x64, 0xFF, 0xFF},
{0x65, 0x00, 0xFF},
{0x66, 0x00, 0xFF},
{0x67, 0x20, 0xFF},
{0x68, 0x00, 0xFF},
{0x69, 0x0A, 0xFF},
{0x6A, 0x44, 0xFF},
{0x6B, 0x00, 0xFF},
{0x6C, 0x00, 0xFF},
{0x6D, 0x00, 0xFF},
{0x6E, 0x00, 0xFF},
{0x6F, 0x00, 0xFF},
{0x70, 0x03, 0xFF},
{0x71, 0x20, 0xFF},
{0x72, 0x00, 0xFF},
{0x73, 0x00, 0xFF},
{0x74, 0x00, 0xFF},
{0x18, 0x00, 0xFF},
{0x09, 0x24, 0xFF},
{0x1E, 0x10, 0x10}, /* Set Bit 4 */
{0x30, 0x00, 0x08}, /* Clear bit 3*/
{0x30, 0x08, 0x08}, /* Set bit 3*/
{0x0D, 0x20, 0x20}, /* Set bit 5 */
{0x09, 0x20, 0x20}, /* Set bit 5 */
{0x1E, 0x80, 0xE0}, /* Write 0x04 to bits 7:5 */
{0xFF, 0xFF, 0xFF},
Thanks,
Sean.