Part Number: DS90UB948-Q1
Other Parts Discussed in Thread: CDCS501
Hello,
We have the following configuration:
MIPI DSI => DS90UB941 => 1 single ended FPD link => DS90UB948 => LVDS screen (800x1200 at 60 fps)
PCLK = 72MHz
The screen have a modulation requirement between 23kHz and 93kHz with a maximum rate of 3%
- In our previous setup we were using an external oscillator to meet the FPD link jitter requirement. The modulation measured at the LVDS CLOCK of the 948 is 12kHz which is below the screen requirementThis cause abnormal display on the screen. The color rendering is abnormal.
- If we use the MIPI clock, we are compliant with the screen requirement (30kHz modulation), but we are not compliant with FPD link jitter, which provide some lock issues and flickering
Questions:
- Do you have a spread spectrum clocking option on the LVDS output of the 948 ? According to our measurement the 948 have a natural SSC.
- If not, do you have a solution to meet the modulation requirement (LVDS retimer ....) ?
Best regards,
Alexandre