Part Number: DP83TC811S-Q1
Other Parts Discussed in Thread: DP83TC811
Hi Team,
May I ask the following questions?
1: Regarding entering deep sleep, is it only necessary to supply 3.3v to VDDA and pin11? And PIN22 VDDIO can not supply 1.8v. Because we need deep sleep uA-level power consumption.
At the same time, there is an Ethernet remote wake-up function requirement. Basically, the power is off, only sbc has a 3.5V output. Need to confirm whether 1.8v can not be supplied during deep sleep.
2: If DP83TC811S-Q1 does not support deep sleep, only 3.3v power supply, please recommend a deep sleep chip with remote wake-up function. Need to realize the vehicle Ethernet function, the interface is RMII or RGMII.
3: DP83TC811S-Q1 is remotely awakened in deep sleep, which one of the INH signal and INT signal has changed, and from what level and why?
4: What is the power domain of the INH signal?