Part Number: DS90UB953-Q1
Hi experts,
I use ub953Q1 to compatible with ub934, follow the document SNLA270A: DS90UB953-Q1 Backwards Compatibility Modes for Operation With Parallel Output Deserializers.
Whether ub953 is possible to transfer MIPI CSI with data YUV422 8bit to ub934? Because i have noticed that in the doc "3.2 BC and Status Settings", it says:
DS90UB953- Q1 only supports 10 bit or 12 bit RAW or similar formats in backwards compatible mode. Formats that fall in same structure as RAW10 or RAW12 can be supported. For example, there are 3 YUV types that have the same pixel packing as RAW10 and can also be used: YUV420 10 bit, YUV420 10 bit Chroma shifted or YUV422 10bit. Register 0x10[2] should be set to one in these cases. YUV 8 bit formats are not supported as the CSI-2 pixel packing structure is different from that of RAW10 or RAW12
Thanks,
Hutian