Other Parts Discussed in Thread: TS5MP646
We need a MIPI switch for a new design. As far as I now, TS5MP646 is a 2:1 MIPI switch for both DPHY and CPHY. However, the pads are too near to place the trace, and they have to use buried blind via. Can TS3DV642 be used as a MIPI switch for both DPHY and CPHY ? Can the unused I/O signal pins leave floated, or they should be connected to ground through a 50 Ω resistor?