Hi,
We are testing our DS90UB960 SubBoard to work with IMX6Q main board. We got an error that IMX6Q processor failed to receive a valid MIPI DDR clock signal.
(1)Probing MIPI CSI clock pin, we found that DATA PINs have an amplitude of 800mVpp,while CLK pins have a amplitude of 100mVpp(400Mbps lane speed).
(2)Data and clock signals have the same routing path.
My questions are:
(1)Are the driver strength of data pins and clock pins same or not?
(2)Can we enforce the drive strength of MIPI clock pins?