Hi Experts,
When 953 is paired with 934, it seems the DVP mode only support 10-bit or 12-bit data type. Is there any workaround to supports YUV422 8-bit when 953 paired with 934? Thank you very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
When 953 is paired with 934, it seems the DVP mode only support 10-bit or 12-bit data type. Is there any workaround to supports YUV422 8-bit when 953 paired with 934? Thank you very much.
Hi Arie,
YUV422 8bit isn't supported in DVP mode. The only way to make this compatible is to configure the SoC to support a different data type.
Jiashow