Part Number: DP83TC811R-Q1
Other Parts Discussed in Thread: DP83TC811
Hello,
We have two DP83TC811R-Q1 PHYs connected between a switch and processor. These PHYs have a transformer-less connection and are on the same board.
The processor is running linux. On board power up if i query the link status using ethtool it says link not detected. All the status LEDs on both PHYs are OFF.
If i take a long piece of wire or an oscilloscope probe and touch C201 (or any other capacitor on the link) the link state immediately goes to link detected and the
LEDs light up. Sometimes this is not required on power up and the link automatically goes up. The behavior is therefore unpredictable.
However, once the phys startup no issues are observed and the connection is stable for continuous operation.
Has anyone faced this issue before ?
The circuit and the PCB routing is shown below. The traces are differential with 100 Ohm impedance. The left PHY is the switch phy and the right one is connected to the processor.
Thanks & Regards