Part Number: DP83822IF
Hello,
I am trying to get a design that has a DP8322IFRHBR to pass ESD. I would like to isolate the drive of the LED's through a buffer such as an LVC1G08, but the LED's are also used for bootstraps. Further complicating things is the fact that the DP83822IF can be configured for either Fiber or copper modes based on the bootstrap resistors placed on the two LED's. How can I place a buffer on teh LED's in a way that it will not mess up the device booting? When the unit is hit with ESD, the PHY locks up and cannot recover unless the unit is power cycled. Can the device be booted by software? This would make things much easier?
Thank you for your help and support.
Jeffrey Cohen