Part Number: ONET8551T
I am testing a number of photoreceivers assembled from the ONET8551T and a photodiode, using long rectangular optical pulses (e.g. 100 ns duration) with a low duty cycle (e.g. 100 kHz repetition rate). The measured transimpedance remains below 1 kOhm as input signal current drops from ~100 uA to about 5 uA (as measured during the rectangular pulse -- this is not the time-average current but rather the peak current during signal pulse reception). Based on Figure 10 of the datasheet, I would expect the transimpedance to increase to a maximum of about 10 kOhm as the signal current drops. However, I understand that my test signal is quite different from the use case for which the TIA was designed (high-rate telecom bit streams). Is it expected that the AGC would keep the transimpedance low for this type of test signal?