Other Parts Discussed in Thread: DRV8305,
To the brilliant electrical engineers out there - could you please help troubleshoot a CAN issue I'm having on my hardware?
I have two boards that are being used to commutate a motor - one board is the Driver Board which contains the MOSFETS and DRV8305 Gate Driver and the other is the MPU board which contains the C2000 chip, CAN transceiver, Rotary Encoder, and associated peripherals.
Code is being generated via Simulink and then flashed to the C2000 via Code Composer Studio with a TMS320-XDS100-v3 JTAG emulator.
For an unknown reason, the CAN will drop out either between board flashes or between power cycles of the hardware..
If you're willing to help troubleshoot, just let me know what additional information you'll need for brainstorming potential root cause.