Part Number: DS90UB948-Q1
Hi team,
could you help to review the schematic about DS90UB948-Q1. Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
Hi team,
could you help to review the schematic about DS90UB948-Q1. Thanks in advance.
Hi Betty,
I will review the file and get back to you in 3 days.
Best Regards,
Charley Cai
Hi Betty,
1. The Ser side and Des side AC caps need to have the same value. Please make sure the Ser side uses 33nF cap as well.
2. The device is a 948 with OLDI output but has CSI output pin names. Please make sure these names are corrected.
3. Please follow datasheet Typical Connection Diagram on selecting the power decoupling cap values.
4. Please use 10uF cap on PDB Pin.
5. Please make sure the OLDI outputs +/- pairs are terminated with 100ohm at the display side.
Best Regards,
Charley Cai
thanks Charley,
customer have update the schematic, please help check it again. thank you.
Hi Betty,
Do you know why they have LL3, LL5 and also has LL13 and LL14? The schematic is ok but this may create layout challenges. They would need to ensure the stub is minimize at the joint point between the two LLs.
Best Regards,
Charley Cai