Part Number: DS90UB960-Q1
My host is qualcomm 820 board which is configured as below
active width = 1920,
actv height = 1080,
line_length_pclk = 2170,
frame_length_lines = 1210
vt_pixel_clk = 78771000,
op_pixel_clk = 266666667,
fps = 30.
Currently, I am trying to generate a Test pattern from the Deserializer with the following configurations
WriteI2C(0x20,0x30)
WriteI2C(0x1F,0x02)
WriteI2C(0x33,0x03)
WriteI2C(0xB0,0x00) # Indirect Pattern Gen Registers
WriteI2C(0xB1,0x01) # PGEN_CTL
WriteI2C(0xB2,0x01)
WriteI2C(0xB1,0x02) # PGEN_CFG
WriteI2C(0xB2,0x03)
WriteI2C(0xB1,0x03) # PGEN_CSI_DI
WriteI2C(0xB2,0x2C) # RAW12
WriteI2C(0xB1,0x04) # PGEN_LINE_SIZE1
WriteI2C(0xB2,0x0B)
WriteI2C(0xB1,0x05) # PGEN_LINE_SIZE0
WriteI2C(0xB2,0x40)
WriteI2C(0xB1,0x06) # PGEN_BAR_SIZE1
WriteI2C(0xB2,0x0B)
WriteI2C(0xB1,0x07) # PGEN_BAR_SIZE0
WriteI2C(0xB2,0x40)
WriteI2C(0xB1,0x08) # PGEN_ACT_LPF1
WriteI2C(0xB2,0x04)
WriteI2C(0xB1,0x09) # PGEN_ACT_LPF0
WriteI2C(0xB2,0x38)
WriteI2C(0xB1,0x0A) # PGEN_TOT_LPF1
WriteI2C(0xB2,0x04)
WriteI2C(0xB1,0x0B) # PGEN_TOT_LPF0
WriteI2C(0xB2,0xBA)
WriteI2C(0xB1,0x0C) # PGEN_LINE_PD1
WriteI2C(0xB2,0x0B)
WriteI2C(0xB1,0x0D) # PGEN_LINE_PD0
WriteI2C(0xB2,0x93)
WriteI2C(0xB1,0x0E) # PGEN_VBP
WriteI2C(0xB2,0x40)
WriteI2C(0xB1,0x0F) # PGEN_VFP
WriteI2C(0xB2,0x40)
When I view the pattern, I get a single bar spread out to width of full screen as expected and then the application crashes. I will post the application issue on qualcomm thread, but I just wanted to be sure that my configuration for 1920x1080 @30fps RAW12 Datatype is configured correctly and there is no issue there.
Additionally, Can someone answer the following questions
-> Can we generate a 4K resolution pattern on this deserializer ? If so, Can I get the configurations for the same?
-> How do we consider the Horizontal blanking and clock speed? Or is it configured to what the host expects?
Thanks in advance,
AG