Part Number: DS90UB947-Q1EVM
Is there a way to create default settings for the eval board so that I do not need to set all of the registers each time? For example some way to store these settings in the microcontroller so that it automatically loads them on power up? Or can I have access to the microcontroller code so that I can modify it to default to the values I need for the mock-up design I am doing with the eval board?