Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP, USB2ANY
Hello,
I have designed 2 PCB's using a DS90UB953 and 954 chip, the ser is powered via Power over Coax. I can see that the 2 chips are connected because the Lock pin is high, and when using the USB2ANY module with the latest version of the ALP software I can see that the 953 is connected to port 0 with an I2C Address of 0x30. I can successfully read the registers of the 954 but I am unable to get any data from the remote registers tab. I have tried playing around with different register settings on the 954 but I have not had any success so far. Can you please give me the register settings for the 954 that will allow me to read the registers of the 953 using USB2ANY?
Thanks