Part Number: DP83867IS
Hi team,
Another customer asked about DP83867, sorry to disturb you again.
The customer problem is described as follows:
1. FPGA and PHY chip are connected through SGMII interface, and a PCS IP core is used in FPGA. During the test, PHY chip is configured as self loop mode, and PCS IP core has a state output signal LED_ LINK( this signal indicates a successful link synchronization). After downloading the program, the link and test are normal. The received data is also correct after comparison. After running the program for about 1 minute, the received data has an error. At this time, it is found that the LED will be pulled low. Under normal circumstances, it should be always high. Then, the signal will be sometimes high, sometimes low, and the received data is also wrong.
In addition, once this kind of phenomenon occurs, as long as the power is not turned off and the program is downloaded many times for testing, the error of receiving data is the same. The error of receiving data will be different only if the power is cut off and powered on again.
2. pin3 and pin9 should supply 2.5V power, but when 2.5V is not connected, there will be about 3V voltage. After connecting 2.5V, the two pins are still about 3V.
The schematic is as follows