Part Number: TLIN1029-Q1
Hello team,
The datasheet says that if enable function is not used, EN pin should be pulled up with between 1kohm and 10kohm.
But EN pin has also internal pull-down so customer don’t think pull-up resistor is needed.
Could you advise why pull-up resistor is needed at disable function of EN ?
Are there any concerns when EN is tied to 3.3V directly ?
Thank you and best regards,
Michiaki