Part Number: TUSB4041I
Other Parts Discussed in Thread: TPS2561, TPS2001C
Dear,
My TUSBHUB4041 is recognized by Linux OS , however when trying to connect a USB device I get the following error.
[ 96.606325] usb 1-1.1: new full-speed USB device number 9 using ci_hdrc
[ 96.690232] usb 1-1.1: device no response, device descriptor read/64, error -32
[ 96.882291] usb 1-1.1: device no response, device descriptor read/64, error -32
[ 96.994541] usb 1-1-port1: attempt power cycle
My assumption is that it has to do something with the current monitoring.
I'm using external power supply and I did not implemented VBUS Power Switch (TPS2561).
Therefore I left the OVERCUR pins floating.
Can someone explain me what might be wrong?
Thanks,
Marin