This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD5S116: About resistor between HDMI connector and device.

Part Number: TPD5S116

Hello,

My customer will use TPD5S116 on HDMI application.
The resistor(180 ohm) is placed between HDMI connector and device.
CES_CON pin -> resistor(180 ohm) -> HDMI connector
SCL_CON pin -> resistor(180 ohm) -> HDMI connector
SDA_CON pin -> resistor(180 ohm) -> HDMI connector
HPD_CON pin -> resistor(180 ohm) -> HDMI connector

(Question)
In this case, is there any problem or concern on TPD5S116?
They have a concern of I2C drive capacity on device.

Regards,
Tao_2199