Part Number: SN75LP1185
Other Parts Discussed in Thread: SN75C185, SN75185, , TRS3253E
Currently, I have a customer using back-to-back 20V zener diodes for ESD protection with SN75C185. They have this protection on Rax (input connected to the outside) and Dyx (output connected to the outside).
But they want to switch to SN75185 - because the DS shows this device has internal ESD protection on Rax and Dyx included in the device.
Can you confirm if the SN75C185 has any ESD protection on Rax and Dyx? (From page 3 of the DS, it looks like there is protection - can you confirm if this is back-to-back ESD protection with ~??V clamp capability? (Like 20V) kV-rating?
Can you confirm if the SN75185 ESD protection on Rax and Dyx is back-to-back ESD protection with ~??V clamp capability? kV-rating?
Can you confirm if the SN75LP1185 has back-to-back ESD protection on the receiver inputs and driver outputs (Rax and Dyx)? If so, what is the clamp voltage? kV-rating?
This will be a huge help - thanks.
Darren C