Part Number: TPS65988DJ
Other Parts Discussed in Thread: TIGER
Hello, we are working with Intel on a Tiger Lake based design using TPS65988DJRSHR. Original design was based on Ice Lake ref designs which used this part but we have since moved to Tiger Lake.
I would like to know if there are updates to the Application Customization Tool (Current is 6.1.1) that are relevant, or if we should use the Ice Lake configuration options. The Controller is the same, so we assume it would work as it works with the Ice Lake, but would like to verify.
Further to that, are there any other documents outlining additional relevant TBT3 configuration options? We have looked at slva931a.pdf but it seems only relevant to the 65892 which connects to external TBT3 controllers.
Best Regards