Part Number: TPS65981
Hi there,
I have a TPS65981 set up as a power sink. I have two PDOs set up as sink options. 5V 3A and 9V 2.5A. These are the minimum requirements for the given PDOs.
When i connect to a source capable of the following:
5V 3A
9V 2A
I expect the chip to reject the 9V as the source is only capable of 2A and use the 5V PDO option as this is to specification for that given PDO.
This is not happening. The negotiation picks the non compliant 9V2A.
Why may this be? i know power wise this may be the larger PDO, but it is still not able to meet the minimum requirements so it should use the 5V.