Part Number: DS90UB940N-Q1
Other Parts Discussed in Thread: SN3257-Q1
Hi team,
customer want to use DS90UB940N-Q1 paired with two different serializers, one from SRV(720p,60fps), the other from DMS(720p,60fps).
They wonder:
1. whether 940N can only output one of the video stream in the same time?
2. if yes, whether change 0x34[4-3] between 10 and 11 online to realize the switch between SRV and DMS? no other configuration needed?
3. they only use one TX port(single channel CSI) now, whether it is ok for this application?
thanks!