Part Number: SIGCONARCHITECT
Other Parts Discussed in Thread: USB2ANY, LMH1297
Greetings,
I have connected a USB2ANY dongle to a customer board using several LMH1297 devices. I have successfully connected to 1 of the devices using SigConArchitect, but the other 3 provide some incorrect register values and do not behave correctly. I believe I have an SI issue with the I2C bus and would like to slow it down to 100kHz. My default sigconartitect using 400kHz and does not provide an option to set the I2C frequency. Is there anyway to do this?
Thanks