Team,
I need help on to bias the input of DS90LV048A, pin 1 and 2 so the output pin 15 to be at logic low.
Right now I have 75 ohms resistor connects between ground and pin 2 of U93 and 155 ohms resistor connects between +3.3V to pin 1 of U93.
Pin 1 measures about +1.8V and pin 2 measures about 0.8V but the output pin 15 is still at logic high 3.3V.
How can I make the output to go to logic low?
Below is snapshot for your reference.