This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: Boot Strap Pin Configuration for Fiber

Part Number: DP83869HM

Hello, I am looking at the datasheet page 44 of the DP86869 to configure for Fiber mode.

I understand Boot Strap Pins RX_0 and RX_1 which set the PHY address.

[RX_D2, RX_D3, JTAG_TDO/GPIO_1]  are set to [0, 0, 1] for RGMII to 1000-Base-X

LED_0 is 0 for Auto-negotiation ON

LED_1 is 1 for Configure Pin 24 as Signal Detect Pin

The question I have is what to do with RX_CTRL, RX_CLK and LED_2.

Can anyone help me please?

Thank you,

Joe