Part Number: LMH0307
Other Parts Discussed in Thread: LMH0324
Hi Sir,
A customer want to confirm the Single-ended input impedance of LMH0307.
it looks like 50ohm on Single-ended input from EVM, Can this device input 75ohm signal?
BTW, can this device output two channels Single-ended on ports of SDO0/SDO0 or SDO1/SDO1?
If this device can not input 75ohm Single-ended, can you provide a recommended devices on application.
Application:
input 75ohm Single-ended signal and output Differential signal two channels 100ohm.
Thanks.