Part Number: DS90UB948-Q1EVM
Other Parts Discussed in Thread: DS90UB949-Q1EVM, , ALP
DS90UB948-Q1EVM Problem working with DS90UB949-Q1EVM
Hi,
I'm now in trouble to work with SerDes.
I used DS90UB949 as a Serializer, and DS90UB948 as a Des. Both are EVM kit.
Here's my condition.
Input : HDMI from PC.
Serializer : 949 EVM
Deserialzer : 948 EVM
Connection: single lane (only 2-coax cable, DIN0+ and DIN0-)
Output : LVDS (dual) to Monitor.
I have a few questions as below.
1. As i understand, FPD-Link III supports not only transfer the serialized data, but also du-plex communication. (for example, I2C, SPI Communication)
That means, serializer must read the status of deserialzer to initialize itself ?
2. I want to transfer the FPD-LINK data by wirelessly. (by using wireless EVM, ST60A2, from STMicro Electornics).
However, our wireless data EVM supports only sim-plex (only forward transfer to the Deserialzer),
I dont want to use auto-initialization of the SerDes EVMs.
3. If i connected SerDes by 2-coax cable, then i checked that Monitor turned on.
At that connection, without touching all the wire connection including power-cable,
i only plug out 2-coax cable and i connected the 2-coax cable to wireless EVM (ST60A2, from STMicro Electornics),
then the monitor turned on correctly.
However, the problem is that, if i use wireless EVM at the first time, without connecting the SerDes EVM by 2-coax cable before,
then it is not working. (monitor is not turned on.)
Therefore, i think that the problem is from the Wireless EVM of sim-plex data transfer.
4. In my situation,
Is there any way to make the initialization of 949 EVM manually ? (like I2C or something.)
I2C address is not changing manually.
How i can change the I2C address of 949 EVM manually?
Very thanks in advance,
Choi.