Part Number: TPIC8101
Hello,
I'd like to ask some questions on how to use the TPIC8101.
- How long does it take for the internal MUX to switch since its SPI register setting?
- What's the purpose/background of having two know sensor interfaces in this device?
- How much frequency tolerance is allowed for the oscillator input?
- Does the TPIC8101 have a start-up sequence of each pin?
- Do you have actual waveform of the input and the output captured with real knock sensors?
- Can the GUI of TPIC8101EVM run on the latest Windows 10?
- Is a simulation model of the TPIC8101 (SPICE model, for example) available?
Best regards,
Shinichi Yokota