Part Number: TUSB8020BEVM
I need it to show feed from two usb2.0 cameras at once (see split screen from two cameras), but it won't work.
I do mange to switch between the cameras feeds as they're both connected to TUSB8020BEVM (meaning both cameras are recognized by PC).
I use default switch configuration: 10010000 (only SW1 & SW4 are ON), and 5V power is connected. LEDS D5-7 are ON, D1-4 are OFF, all jumpers (J2, J7, J8) are connected.
Why can't I see both feed simultaneously?
How to achieve this?
Thanks,
Elia.