Part Number: ONET8501PB
Hello experts,
I have found an odd issue while using the ONET8501PB as the RX for an O/E application. During programming I set the pre emphasis settings on register 2 to a value of 8 (1000), which is not listed as a possible value in the data sheet, and got the following result:
Similar results can be seen when writing for 2 (0010) and A (1010) which are also not listed in the data sheet as possible values. Using a value form the data sheet, in this example C, gives the following result wherein the output power is reduced considerably:
The output from the ONET8501PB when using an unlisted value is more useful for my application but I am worried about possible repercussions as this is not a listed value in the data sheet. Does anyone know why I am getting this output or if there are any design problems that may arise from using unlisted values. This is an urgent issue and has formed a bottleneck in trying to decide if this a valid solution or not so any help would be appreciated.