Part Number: DS90UB934-Q1
Hi,
do you have DS90UB934-Q1 example code can share? or basic settings? thanks.below is schematic thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB934-Q1
Hi,
do you have DS90UB934-Q1 example code can share? or basic settings? thanks.below is schematic thanks.
betty
the sch. design sounds good but anyway please refer to TI's recommendation design in d/s. it is better if you have 100ohms resistor after AC coupling in CMLOUTP/N pin.
regarding the script code, ub934/933 can run up automatically if you have correct mode_sel setting in 934 side. so TI has no special script code for it. if you need i2c remote, you just need enable this function based on i2c over FPD-Link app. note.
regarsd,
Steven