Part Number: TUSB546A-DCI
Hi there,
I was hoping to use this IC for outputting HDMI over Type-C.
I've been looking into USB-C alternate modes and noticed that TI makes a nice little chip for doing muxing (TUSB546A) that can handle the HDMI 1.4b protocol. Currently, I was hoping to port over the PD IC controller (STUSB4500 from STMicroelectronics) I am using which is programmed over i2c via its NVM (which allows up to two PD profiles and on-the-fly PD capabilities if connected to an i2c master). I don't think it handles alternate modes though, and this is where I am getting lost... does this chip require a specific PD controller capable of negotiating alternate mode configurations, or will any old regular standalone PD controller work? I've read the application report below, the schematic showing a PD controller with an inbuilt SBU mux for switching the HEAC/HPD lines - was just wondering the potential options for PD controllers for use in this application.
If my HDMI source doesn't support HEAC, could I just potentially leave these pins floating and pull the HPD high with a 1K resistor to enable HDMI?
Kind regards,
Benjamin