Other Parts Discussed in Thread: TPS65987
If I use two TPS65987 to connect each other, we prefer to avoid Electronically Marked Cable Assembly (EMCA). As I understand the current rating would be limited to 3A.
If I use a passive cable without electronically marked , 60W (20*3) would be maximum power budget?
With 20V as input, can the max power delivery is 60W.
regards
Prabhu