Other Parts Discussed in Thread: TEST2,
In section 9.1 of the datasheet it says the following:
"The SN65DSIx6 is a bridge which interfaces DSI to embedded DisplayPort (eDP). Because it does not support HDCP, it is only intended for internal applications like notebooks and tablets. Four lanes of HBR2 (17.28 Gbps before 8b10b encoding) and dual DSI input (up to 8 lanes at 1.5 Gbps for a total of 12 Gbps) allows the SN65DSIx6 to support large high resolution eDP panels."
I want to drive a DP connector and I don't need the HDCP, so is this ok? Can I drive a connector directly?
Do I have to do something with the TEST inputs to make this work?