Part Number: TPS65983B
Hi,
I am developing a board by referring to Tapex Creek TI83.
I customize the TPS65983B firmware using Application Customization Tool, Do I need to register a USB Vendor Id to use Thunderbolt?
I have no plans to use USB. Only TB3 functions are needed. Nevertheless, do I have to register?
The default value is 0x8087, can't we leave it as it is?