Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987,
Hi All,
We are using TPS65987 in our board, Following are some queries related to this :
1. TPS65987D supports one time programming for specific configuration. So that for each power on cycle / reset of the TPS65987D chip , it would configure itself without any host interaction . This scenario is required in one of system scenario in which host is not available for configuration.
2. We would like to put TPS65987D in "Data Role - device mode" for data and "Power Role - Source mode" for power. ( UFP Power source mode) . Please provide the configuration settings to be used in TI's GUI tool and also if we need to perform over I2C interface through host interface .
3. Does the TPS65987D uses internal flash memory to store the configuration settings and firmware image once configured by TI's GUI tool , please confirm
Provide your quick response as we need to close the design and want to start proto manufacturing.