Dear *,
i was going through SLVAE37
and have some questions regarding two calculations :
1)
"
The SMAJ33A has a RDYN of 884 mΩ, so a nominal VCLAMP = 38.6 V + (24 A × 0.884 Ω) = 59.8 V. This is
the nominal clamping and is very close to the clamping voltage requirement, however we want to ensure
that there will be no issues when surges are applied over temperature. The data sheet does not specify
clamping or breakdown voltage over temperature; however it does provide a temperature coefficient that
we can use to calculate. The temperature coefficient is 10 × 10-4 /°C, so we can calculate VCLAMP at 85°C =
VCLAMP at 25°C × (1 + 10 × 10-4/°C × (TJ
-TA
)) = 59.8 V + (1 + 10 × 10-4/°C × (85°C – 25°C)) = 63.4 V. This
clamping voltage violates the 60 V absolute maximum of the input circuitry.
"
1a) i was trying to find Rdyn in SMA TVS datasheet without success, how to get this value?
1b) VCLAMP = 38.6 V + (24 A × 0.884 Ω) = 59.8 V -> what is the 38.6V and what is the 24A from TVS SMA datasheet?
2)
"
The SMAJ33A data sheet lists nominally that it can withstand 400 W of 10/1000 µs transients, which we can translate to 2300 W of 8/20 µs power by using the data sheet curves."
How can we do that?
Best Regards,
David.