This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS20: Connecting Zynq UltraScal+ MPSoC (HP Bank)

Part Number: SN65LVDS20


Connect the HPbank (1.8V) of the "Zynq UltraScal+ MPSoC" to the SN65 LVDS20.

The output of MPSoC is
VOCM: typ: 1.2V (1.0 to 1.425V)
VODIFF: typ350mV(247-454mV)

The SN65LVDS20 (VCC=3.3V) is
VICM: 1.2 to VCC-VID/2
|VIA - VIB|: 0.08 to 1.0V

Can the SN65LVDS20 operate correctly when the VOCM of MPSoC is 1.0V, as long as |VIA - VIB| is met?