This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB934-Q1: 934 res conflict in datasheet and EVM

Part Number: DS90UB934-Q1

Hi Team,

The datasheet said OSS-SEL need to less than 4.3k, but the EVM is 10k?

Could PIN 34be floating instead of 4.7uF to GND?

  • Hello Amelie,

    about OSS_SEL, it looks like it is a typo in the EVM. The Pull-up resistor is not mandatory, but if you decide to use one, then it should be =< 4.3Kohm.

    No, you can't leave VDD11_FPD floating. It requires a 4.7uF or greater capacitor to GND.