Part Number: TPS65982
Other Parts Discussed in Thread: TPS65987D, TPS25750, TPS65994AD
Hi Team,
This is customer request can you please advise:
"
TPS65982 chips are used mutually in our designs. A flash memory from SPI is connected to this chip.
When I try to access the TPS, I get the information from the SPI that the application firmware cannot be loaded and the chip remains dysfunctional.
Normally the TPS65982 can write to flash, but requires the application firmware to be successfully loaded, and a vicious circle occurs because flash is empty at first.
When I do research to program SPI flash, I see that this is not possible:
This link says the flash needs to be programmed somewhere outside, but that's impossible for us.
How can we program SPI Flash for first use under these conditions, or is there a way to make the TPS65982 functional without programming the flash?
"
Thanks in advance
Best Regards
Furkan Sefiloglu