Part Number: SCANSTA112
I need to configure this TI JTAG Multiplexer (SCANSTA112) in Scan bridge Mode (using the JTAG port). My only JTAG tools are from the Intel Quartus Prime and Micro Semi Flash Pro tools. These tools are FPGA specific and I don't think they can be used to configure the TI JTAG Multiplexer ? What tool do I need to configure this device, a standard IEEE 1149.1 controller ?? Is there a TI application or demo kit that comes with a simple controller that I can use to download a programming file into this device ? I understand this device can be configured by strapping the hardware pins on power up or reset, but that will not work on my application.