Part Number: ALP
Hi, Is it possible to export registers settings to a script file using Analog LaunchPad tool?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ALP
Hi, Is it possible to export registers settings to a script file using Analog LaunchPad tool?
Hi Max,
Are you referring to the direct register or indirect register? If it is direct register, yes you can use the "Save" button for direct register dump.
Aaron
Actually I have not connected the ALP to the hardware and I want to change dump register settings after changing them in GUI. I tried my luck with save button but it is not showing values I have configured.
Hi Max,
In order to save the dump register data, you need to connect the ALP with a physical device such as the EVM. You can't use it when the ALP in demo mode.
Aaron
Hi Aaron, Thanks. I think such feature will be useful as you can generate hardware configuration using ALP tool where EVM board is not involved.