Part Number: TCA9554
When VCC is above 3V, then Vih is 0.8xVCC.
which is higer than my design.
could you recommend other material which have lower Vih.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9554
When VCC is above 3V, then Vih is 0.8xVCC.
which is higer than my design.
could you recommend other material which have lower Vih.
Hi
my power rail is 5V.
Based on my understand, Vih should be around 2.x V
is there any reason TCA Vih is higher than normal Vih. (2.X V)
Dimitry,
Since your VCC supply is 5V, the VIH will be 0.8*5V = 4V. The only way to change this would be to lower the VCC supply.
Regards,