Part Number: TPS65987D
Hi,
I have programmed the flash and the TPS chip does not successfully boot into application mode. It is not obvious what is going on and the existing tools / docs are unclear especially when it comes to steps for commissioning a new board/chip.
Do I have to generate a binary or can I flash from current project?
If I generate a bin file do I need both a full flash and the low region? Or does the full cover both? How are the region offsets determined?
Where do I obtain the latest patch code?
My flash was empty I was attempting to use the GUI and an Aardvark interface but that has not worked. I've also attempted to use the external Aardvark flash tool. Lastly, the HI Firmware update command seems to also be useful but I can't even run it as it usually says Boot Failure and region start addresses of 0x3 if it works at all.
I have ADCIN1 at 1.1V out of 3.3V. The MISO is pulled low. This config has worked on my slightly modified EVM but now I have a new custom board and new empty flash chip.
Thanks,
Chris