Hi, all
We have an issue with LMH1219 IN0/1 and OUT0/1 mux.
Here we set CTLE Page 0x31=3F to declare it is controlled by internal register.
Then we set CTLE Page 0x90=20, 0x1C=98, 0x 1E=29, 0x31=23 to let it input with IN1 and out put with OUT0 and OUT1;
Cable EQ Page 0x30=2A, 0x31=41, 0x32=2A, 0x33=41.
Test data rate is 11.88Gpbs on IN1.
It's very strange that OUT0 can normally output signal, but OUT1 cannot. Only when we connect the pin IN_OUT_SEL to high voltage with all the other hardware control pin float, OUT1 and OUT0 can both work well.